Other Parts Discussed in Thread: ADS131E08
Hello,
I am currently working on a circuit using ADS131E08. For now I am only using 3 inputs for voltage sensing, following the differential set up shown in the datasheet (under "VOLTAGE SENSING"). It works as expected, but I need now to use the fault detection features, to detect that the "L" probe, for example, has been disconnected. Under "FAULT DETECTION" in the datasheet there is a suggestion to use pull up and pull down resistors to trip the signal when the circuit is open. Problem is, when using the topology suggested in the mentioned section, the fault detection messes the signal, and doesn't actually trip the signal because it only makes a resistive network between AVDD and OPAMPOUT. Could you please help me? As mentioned, I am using EXACTLY the same topology as suggested on the datasheet, but I simply cannot get fault detection to work, what am I missing?
Thank you very much in advance.