Other Parts Discussed in Thread: ADS1298
Hello,
I have a question regarding the conection and configuration for using the ADS1298 in an 12 lead ECG system.
Acording to what i have understood from the datasheet:
pin01 (IN8N) - to pin 64 (WCT)
pin02 (IN8P) - V6 (chest lead)
pin03 (IN7N) - to pin 64 (WCT)
pin04 (IN7P) - V5
pin05 (IN6N) - to pin 64 (WCT)
pin06 (IN6P) - V4
pin07 (IN5N) - to pin 64 (WCT)
pin08 (IN5P) - V3
pin09 (IN4N) - to pin 64 (WCT)
pin10 (IN4P) - V2
pin11 (IN3N) - to pin 64 (WCT)
pin12 (IN3P) - V1
pin13 (IN2N) - LA (left arm)
pin14 (IN2P) - LL (left leg)
pin15 (IN1N) - RA (right arm)
pin16 (IN1P) - LA (left arm)
So, I have:
IN1P (LA) - IN1N (RA) = DI (bipolar derivation I)
IN2P (LL) - IN2N (LA) = DII (bipolar derivation II)
Also, my configuration for WCT1 and WCT2 registers is:
WCT1 = 00000001
WCT2 = 00000010
DIII, aVR, aVF, aVL can be calculated.
My question is, are those conections to the pins of the ADS1298 correct for a 12 lead ECG? Do I need con configure something else?
Thanks in advance!!!!!