Other Parts Discussed in Thread: ADS42JB69EVM
Hello TI Community,
I have some questions concerning the ADS42JB69EVM Board. I have the following hardware components:
TSW14J56EVM FPGA Board
ADS42JB69EVM Eval Board
I Installed the High Speed Data Converter Pro v3.0 and the ADS42JBx9 GUI. Everything works fine. But I thought about somehow exporting the Captured Wafeform into a .csv file or something like that. So I put in a Sine-Signal with 1 MHz and set the ADC Data output rate to 250MHz. How can I get the initial sine-waveform back, so the amplitude-values of the ADC. Can I read them out somehow? I only see FFT and BITS options, but thats not the thing I want. I hope you can help me,
Greetings