Other Parts Discussed in Thread: ADS1298
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS1298
Hi Brian,
Thanks for your quick response. I understand that you're unable to provide advice on body testing so I'll not bother you with that.
I'm facing a rather strange problem at the moment that might be linked to the offset produced by the simulator. In the image below, Channel 1 (V6) is suddenly producing a strange waveform that is unusual. This has only started happening today. No changes were made to the code, nor hardware. Could there be any particular why one channel would behave very differently from all other channels (up till 12-lead application) are working just fine.
Again, thank you for your help.
Regards,
Mohd Aslam
EDIT: I checked the STATUS word and can confirm that it is not detecting any Lead-Off for V6 lead nor any of the other 9 electrodes.
Hello Mohd,
From that image, it looks like the lead is not being actively driven. Is the y-axis measured in millivolts? For a proper Lead-Off detection, you'll need to ensure that the control registers contain the right settings. What have you programmed in the following registers: LOFF, LOFF_SENSP, LOFF_SENSN, LOFF_FLIP, CONFIG4?
Regards,
Brian
Hi Brian,
Thanks for your help. I've managed to figure out the problem. It was a trivial issue whereby the CH1SET register was in temperature sensing mode.
I have a question regarding temperature sensing of the ADS1298. Hope it's ok to continue adding questions to this thread without starting a new one. Based on pg. 54 of the ADS1298 datasheet, it says that there is an on-chip temperature sensor. I'm not sure if I'm interpreting it correctly 'cos I'm a little confused.
Is the internal temperature sensor intended measure the temperature of the chip or the patient's body (i.e. electrode) ? Because based on the picture of the Input Multiplexer block, it looks like multiplexing to [2:0] = 100 does not connect the ADS1298 to the VINP and VINN of the electrodes. It selects TEMP and TEMN but i don't see where this goes. With the electrodes connected to the ST-16 ECG simulator, I've tried getting temperature readings and obtained approx. 29 degrees celsius. Putting the electrodes on my hands doesn't change the temperature much.
The ultimate question is, what is the temperature sensor measuring.
Again, thank you for your help.
Best regards,
Aslam