Other Parts Discussed in Thread: AMC1200, AMC1100, ISO122, ISO124
Dear All,
Our recent requirement is to have a channel Isolation of 1000 V between each channels in the 8 ADC inputs. It is a single ended input with the given values as 0-100V or 0-4V or 0-100mV o r 4-20mA input channels.
Please let me know,
- The best suited Analog Isolator ( Isolation Amplifier) for our application from TI ?
- Which isolator is good for our application. Isolation amplifier with Optical barrier or Capacitive barrier?
Best Regards
Sharvy