Other Parts Discussed in Thread: ADS5463, DAC5674, CDCE72010
Good day:
My name is Francisco Eduardo Balart Sánchez and i’m working in a “concept proof” project which involves digital signal processing. The project is in the phase of implementation, therefore I have to research what devices I need for such implementation and how much the “minimum system” would cost. What solution can you propose?
Here is a more detailed description of the project.
I’m trying to implement digital signal processing to an analog RF signal (CATV) with frequency ranges from 5 MHz to 200 MHz, therefore I know I have to implement a ADC then a DSP or FPGA and after a DAC (plus the signal conditioning PLL’s, etc.), but there some things I don’t understand well.
For example since my greatest frequency is 200 MHz (in which I have to recover the carrier) I try to use an ADC with at least more than the double of 200 MHz. I’ve seen some ADC’s which uses undersampling and others not, if the signal content is in al the 5-200 MHz spectrum I have to use a ADC with more or equal than 400 MSPS? Or is there a way to achieve this with undersampling?
After I choose then an ADC then I don’t know the relation of the clock needed to achieve such SPS. What is the relation between the samples per second and the ADC’s clock?
Finally the DSP or FPGA selection must meet the speed of the ADC (in the I/O bandwidth specification)
I hope the previous explain a little bit more the scope of the needs in order to help you to propose a solution (minimum system including clock, PLL, VCO, DAC, etc.).
Thanks in advance and best regards
M.S. Francisco Eduardo Balart Sánchez
dkbf73@motorola.com
Ph. +52 (81) 1301-0215