Part Number: DAC8560
Other Parts Discussed in Thread: OPA188,
Dear team
I use the internal reference of the DAC8560 and amplify the output to 0-5V through an op amp. Is my circuit correct? Whether the op amp OPA188 and DAC8560 are stable. Is 1nF suitable for C90 capacitor? Can the output of the op amp be protected to avoid damage to the follow-up circuit when a fault exceeding 5V occurs.