Part Number: ADS1282EVM-PDK
Other Parts Discussed in Thread: ADCPRO, ADS1282
Hi,
I would like to ask you some question about the ADS1282EVM-PDK module that I'm currently controlling with the ADC_Pro software.
Is there any software to manage directly low level commands to access registers , so I can easily monitor the ADC interface with the oscilloscope and try to clirify some doubt ?In particular, it seems that I cannot control the SYNC command and the RDATA command with the ADC_Pro, is that correct?
I'm going to implement on FPGA a driver to control only one ADC, but I need to trigger the start of the acquisition on a particular event; so, I was planning to drive the SYNC pin or send the SYNC command, to start a new acquisition. Do I have to send also the RDATA command after the SYNC, or the /DRDY signal will be asserted as soon as a new data is available after the syncronization process and the data can be shifted out?
Since I'm going to use both analog input channels, I'll set the internal mux by means of CONFIG1 register. Does this write access restart the ADC acquisition so I do not need to use the SYNC command after that, but only the RDATA command? I'm confused about the RDATA command, since I do not understand if it's just a command to transfer the acquired data on the output buffer to be shifted out, or if it start a new acquisition proccess as well.
Do you have suggestion on wich command sequence should I use?
Thanks for you help
Viviana