I´m working with the ADS131E08 using SPI to communicate with stm32f765IG and after correctly configuring the device and start conversions
1. initialization procedure is performed in accordance with the datasheet
2. ID Control Register = 0xD2
3. Config3 = 0xCC
4. All the available commands are executed correctly
5. Output data rate <= 16 kHz, 24 bit mode
i experience a deterministic issue which is i expect to receive values in my buffer these values are {0xD2,0xB2,0xE0,0xCC,0x00,0x10,0x10,0x10,0x10,0x10,0x10,0x10,0x10,0x08,0x00,0x00}
if(au8Registers[u8Index] != astrRegisters[u8Index].u8Value)
{
/*
rest of the code
*/
}
but the ADS chip doesn't send back these values in a definite time sometimes i wait for a long time to get the data red properly .
if i changed the spi clock to any value but 5.6 MHz i dont get the values ever .
the chip doesnt respond as it should be even when am performing the configuration in accordance to the data sheet and its not deterministic
please help me