This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4249EVM: Problem with the activation of digital functions (gain, offset correction, test patterns) of ADS4249 on ADS4249EVM

Part Number: ADS4249EVM
Other Parts Discussed in Thread: HSMC-ADC-BRIDGE, AFE5809, AFE5809EVM

I am working on a similar project , but instead of using an ADC, I am using AFE5809 EVM to configure Cyclone V GX starter kit via HSMC-ADC-Bridge.

Can anyone help me in the interfacing of above components.

The basic idea is to pass analog signal to AFE and then pass the digitized signal to FPGA through HSMC-ADC-bridge.

Do we require TSW1400 EVM for this?

Also how to convert differential ended signal output from AFE to single ended output.

can we control the triggering operations through FPGA like can it control AFE on when to start the conversion and send data and when to stop it.

Regards

Shyam