Hello,
I have the new plugin of ADS1147 and the driver is correctly installed.
1. Install ADC pro and EVM plugin (and the driver)
2. Connect the ADS1248EVM to the MMB3 and the SW4 of the MMB3 in the right position
3. Connect the MMB3 to my PC via USB (BRD TEST message appears)
4. Start ADC Pro
5. Load ADS1147 EVM plugin
6. The software find the MMB3 and the message "Switch to the BSL position then press ok" appears
7. I switch to the BSL position (BRD TEST message disapears)
8. I press ok
9. "An error occured with error code" " or "improper BSL version !" message
Could someone help on this issue?
Thank you.