Continuous-sync mode with Sync clock does not work.
DOUT always outputs 0.
ADS1282 settings are as follows.
- CONFIG0 Register: 0xC2 Continuous SYNC mode, 250SPS, Sinc + LPF filter.
- RDATAC command
- Sync signal: GPS TP(Time pulse) signal 250Hz.(This signal is very precious sync signal.)
If the GPS TP signal is not input, DOUT is output normally.
I changed the sync signal to a different value and tried to input it as the original value, but it still does not work. (ex: 300Hz -> 250Hz)
I want to operate it as in Figure 48 on page 23 of the datasheet, but it does not work.
Best Regards,
KJ Park.