Part Number: ADS7828
Hi
I am testing one A/D converter circuitry with ADS7828EB installed. As part of my test procedure I need to apply 2.87 V for 50 mS to the analog channel. VDD for the IC is 3.3V and REFIN/REFOUT pin is connected to GND using and 0.1uF capacitor. It looks to be OK to apply 3.3 V as an absolute input as per Datasheet. Can somebody please confirm my test conditions will not harm the ADC
Nimmy