Other Parts Discussed in Thread: ADS1278, CDCE906
Dear experts,
I'm in the design phase of a new board where the main components are OMAP L138
and ADS1278. We have some doubts and I hope your experience will help us highlight
possible problems. First of all our system has to adjust dynamically the
sampling frequency from few kHz to the top converter speed (144kSPS).
We checked the schematics of EVM module and carrier, but we still have
doubts both on hardware and software sides;
Here a list of questions.
Hardware:
1) On the ADS1278 datasheet (July 2009) at page 5 is stated DVDD has to be
between (1.65 - 1.95) V if fclk is less then 32.768 MHz and between
(2.0 - 2.2)V over that frequency. Does it imply DVDD has to be changed
dynamically? Can it be fixed at around 2 V in any case? Can you detail
possible drawbacks? In the ADS1278EVM DVDD is fixed at 1.8 V, does it mean
it cannot run at top speed?
2) Considering the interconnection between the converter and the processor
we are planning to use the McBsp port. We have few dubts regarding this
interconnection:
a) is the McBsp fast enough to manage continuously all the data acquired
by the converter? Would the McASP (we have few experience with it)
coupled with the converter in Discrete output mode a better solution?
b) Considering the McBSP case, what is the best topology for the clock generation.
Our first guess was using the schema at page 38 of the ADS1278 Datasheet
(is the flip flop necessary?). In this schema the CLKR is an output. Our doubt is: can the
L138 generates all the desired frequency on CLKR to drive the converter?
What will be the jitter on the generated clock? and the accuracy?
Unable to find out answers, we investigated the possibility of adding an
external programmable PLL (CDCE906 for example) to generate Clk and drive
with it both CLKR and SCLK. In this case we are able to generate all desired
frequencies, but the power budget is very critical for us. Is the external
PLL necessary?
Software:
1) We are planning to use the ARM side alone in the first stage. Our hope is running Linux
because we need some services (mainly networking and file system). Is there enough
horse power in the L138 to continuously acquire data at converter's top speed and
stream (eth) or store (sata, usb) them?
2) Is there around something similar to
http://processors.wiki.ti.com/index.php/OMAP-L1x/C674x/AM1x_Multichannel_Audio_Serial_Port_%28McASP%29_Throughput_and_Optimization_Techniques
with benchmark, examples and suggestions for McBsp?
Best Regards,
A.