This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Program "make" is not found in PATH



Hello All,

I am presently using CCS  Version: 5.1.1.00031. I have included MCDSK also.During build i am getting error, Program "make " is not found in path. I have copied the screen shot of the error.

Thanks in advance.

the

  • Have you tried reimporting the project into a new workspace? There were some known issues in 5.1.0 where importing certain projects created on a older version caused gmake to be replaced by make in some cases. This was supposed to be fixed in 5.1.1 though. Please take a look at this related post regarding this known issue and how to resolve.

    If using a new workspace or the workaround suggested in the other thread does not help, can you provide us with the project that reproduces this issue?

  • Thanks AartiG for the post and when the tab is selected its working fine.

  • HI,GS,

    I met the same problem you had met.can you give me a clear direction about solving it .

    is it the ccs vision is too low?,mine is ccs5.1.

    and i counld not find the selected button the hearty TI employor had said ..

  • Hi Baoyi Han, 

    Long before i have placed into another project, I do not remember what i did, but looking into the previous posts, i understood i have followed what   has suggested.

    I am copying that link to you and hope this would help you.

    Please take a look at this related post regarding this known issue and how to resolve.

  • To the specific problem, inside the project properties -> Build -> Builder, you can check "use default build command" to remove the make command.

    The broader solution is to import the project from the Project drop down menu. Opening the project normally will leave things like make as the build option. Importing the project seems to auto-correct this things.