Hi Champs,
I'm trying to use the on-board XDS200 on my K2 EVM. I'm running under Ubuntu 13.04 64-bit. Emupack is ti_emupack_keystone2_setup_1.0.0.3.bin When connecting I get the error:
Error initializing emulator:
(Error -2083 @ 0x0)
Unable to communicate with the emulator. Confirm emulator configuration and connections, reset the emulator, and retry the operation.
(Emulation package 5.1.73.0)
The log file says:
E 04/23/13 10:51:25:929 | rpcenv.cpp(1299) E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
XDS560v2 works fine with the same board under Ubuntu.
XDS200 works fine when using from Windows 7 machine.
Kind regards,
one and zero