This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS200 issues on Linux CCS 5.4



Hi Champs,

I'm trying to use the on-board XDS200 on my K2 EVM. I'm running under Ubuntu 13.04 64-bit. Emupack is ti_emupack_keystone2_setup_1.0.0.3.bin When connecting I get the error:

Error initializing emulator:
(Error -2083 @ 0x0)
Unable to communicate with the emulator. Confirm emulator configuration and connections, reset the emulator, and retry the operation.
(Emulation package 5.1.73.0)

The log file says:

E 04/23/13 10:51:25:929 | rpcenv.cpp(1299) E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io

XDS560v2 works fine with the same board under Ubuntu.

XDS200 works fine when using from Windows 7 machine.

Kind regards,

one and zero