This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6748 CCS5 XDS510USB connection issue PRSC failed , -6305

Expert 6160 points

Hi , a customer is trying to use XDS510USB on new board having c6748.

They already tested emulator with zoom board + another custom one

On this new board , despite Emulator test is ok (scan test) + ICEPICK connection ok , it fails with following error

"Error Connecting to the target : Connect to PRSC failed , -6305"

Can you please help with possible reasons for this

1/ Would you know the error type and reason of -6305 ?

2/ anything to check on the hw lines (reset ones, clocking)  ?

Thanks

Nicolas