Hello
I use XDS100v2 20-pin TI connected with my board (beaglebone black), without JTAG header. I soldered 20-pin cable directly to the board and connected to XDS.
It looks like this:
When I start "Test connection" in "Target Configuration", i get an error: 'SC_ERR_CTL_NO_TRG_POWER'
I checked each pin and on 5-th pin 3.48V. Or, i can't connected JTAG like that?
Best regards,
Svyatoslav