I am using C2000 Emulation Flash 1.0.0.2
Currently I am unable to connect to the CLA Type 1 on F2837xD C2000.
The DEBUGCTL register is not being configured properly when the debugger is connected. the SSE bit is not being set when I connect to the CLA with the debugger.
Maybe an update introduced a bug into this.
sal