This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have an Spectrum Digital C2000 Series XDS510LC emulator. The users guide says that it's driver is already installed as part of CCS 3/4/5. But when I tried to use it for the latest CCS 6.1, I don't see it listed in the Connection list. Is it still supported or where I can download driver to get it to work for my F28377D controlCard? Many thanks for your help!
Shef said:Do I have to re-install the entire CCS 6.1 in order to include it?
You do not need to reinstall entire CCS. You can simply re-run the installer exe, choose the installation directory as the same directory where you previously installed, and then select the components to add on, specifically the Spectrum Digital drivers.
Hi,
Another reference to add components to an existing install is shown in section 3 of the page below:
processors.wiki.ti.com/.../Updating_CCSv6
Cheers,
Rafael
Shef said:However, when I tried to use it to program/debug my F28377D controlCard, it failed and error out on me. In there "Connection" list, there is an option called "Spectrum Digital C2000 XDS510LC Emulator" which is exactly what I have for hardware. But when I selected it, it immediately pops up an error dialog "Unable to find an appropriate device driver for the connection type "SD2000USB" and isa "ICEPICK_C". Then I selected "Spectrum Digital XDS510USB Emulator" in Connection box, and F28377D for Device. I saved and tested connection, which was successful, showing 1 JTAG IR and 1 device found. But when I tried to program/debug a known good project, it failed with error box "Failed to Initialize IcePick_C_0".
I can confirm that I see the same error with my installation as well. Unfortunately Spectrum Digital XDS510LC emulator does not seem to be supported with F28377D devices.
Please see this related thread for more details. I also found some information on an internal discussion where Spectrum Digital confirmed that they do not have plans for any XDS510xxx class driver updates to add support for Icepick.
Very sorry about the inconvenience caused by this, but you would need to go with one of the other emulators mentioned in the referenced thread.