This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6746: Can't install Blackhawk drivers

Part Number: TMS320C6746

Tool/software: Code Composer Studio

I am installing CCS 8.0.0 and I am selecting Blackhawk Emulators support during the installation. At the installation time, USB-560M wasn't connected to my PC. I have connected it after the installation, which started the automatic driver installation, which failed without any extra information except that it failed. Then, I checked the status of the emulator in the Device Manager, and the status was that the driver can't be installed because "System cannot find the file specified" without any reference to which file was missing.

I also tried to follow instructions from the Blackhawk control panel, and after I clicked on Reinstall All ... button, I got the error message "Update Driver failed ! Error: Access is denied”.

I have tried different USB ports, reinstalling CCS with the emulator connected, but none of these helped. I was mainly running in circles getting these same error messages again and again. What should I try next?