Tool/software: TI C/C++ Compiler
I have occasionally seen George Mock say something like the following, for example in https://e2e.ti.com/support/development_tools/compiler/f/343/p/624681/2306594#2306594:
TI has never documented that bit identical object files will result from multiple builds with the same conditions. We don't test for it. Therefore, it is not wise for you to rely on it.
This statement only applies to object files, correct? .obj and .lib and .out files?
We need to be able to verify that our binary images can be built and rebuilt identically; that our images built on our developer machines match those built on the build server, and that we can rebuild identical code later on and create an identical binary images. Where by "binary image" I mean just the binary code/data that gets programmed into our MCUs, not any metadata for debugging or otherwise. Our first preference for validating this would be to generate identical .hex files. We don't have any particular need to verify .obj or .out files. (I appreciate that the objdiff tool is available if this verification need were to arise.)
Does TI officially support generating bit identical binary images from multiple builds with the same conditions?
(Is there a phrase you would prefer to use other than "binary image" to capture this concept?)
We're specifically interested in TI's ARM compiler while compiling C code.
When we speak of "the same conditions", what are those conditions? Of course we need to use the same version of compiler and linker. (We'll certainly use the same version of the hex conversion utility as well, although I'd hope that that would be quite compatible across a range of versions.)
I am hoping that we do not need to:
- Use identical absolute directory paths for the root directory of our CCS project.
- Use identical absolute directory paths for the installation of CCS and the compiler.
- Use the same version of OS. (Meaning the OS we run our build environment in, of course, not any RTOS we might compile into our binary image.)
- Use the same kind of CPU or any other hardware on the computer running the build environment.
Certainly we need to be careful about embedding timestamps and datestamps. We will plan on avoiding __TIME__ and __DATE__ macros. I don't believe TI provides any way to control those values, correct? It would be useful to support a way to control those, potentially using the SOURCE_DATE_EPOCH environment variable supported by GCC.
I don't believe that we need to worry about any C locale issues, because those are hard-coded to the C locale in the TI library, correct?
We will consider placing the compiled run-time library into source control. Do you recommend doing so? Even if we do, we would still want to follow whatever approach we need to do such that we could get a repeatable build using the default CCS approach (i.e. using the run-time library compiled from scratch in the tools directory).
Are there other pieces we need to explicitly control in order to reliably generate repeatable binary images?
--thx