This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can we connect TPS22963C switches in parallel. When ever the switch is disabled will it ground the line. And some times I want to connect a external source at the output of the switch will the switch allow current to pass through ground when it is disabled like TPS22960. When I am trying to simulate I am getting convergence error what does it mean.
Hi Chaitanya,
I am going to move this question to the modeling forum so that they can comment on this.
Thanks,
Alek Kaknevicius
But when I am trying to simulate it is showing convergence error. Also my current rating is at max 500-600mA, But the switch rating is 3A. Is it fine to use that in this application. I am attaching the simulation model can you verify that. (Enable each and every voltage 3.3,5,1.8) Also enable pullup switch. TPS22963C.TSC