Other Parts Discussed in Thread: DLP3010, , DLPA2005, DLPC3438
I am using the DLPC3433 with DLPA2005 and DLP3010.
I currently have everything setup and see the DLPC communicating over SPI with the EEPROM chip.
The VOFS, VBIAS, and VRST are at the correct voltages.
HOST_IRQ stays high which means the DLPC hasn't finished initializing.
I have already found a mis-wiring in my custom design for the high-speed DMD pins. However, will this mistake keep the whole board from operating ?
I know at this point the video won't work. But is this issue what is keeping HOST_IRQ high or is that a different issue?
DMD_DEN_ARSTZ, DMD_LS_CLK, DMD_LS_WDATA, DMD_LS_RDATA are routed fine.