Other Parts Discussed in Thread: DLPC7540EVM, DLP471TE, DLPC4422, DLP650TE, DLP651NE, DLP471NE, DLPC7540
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lidong,
The DLP471TEEVM requires the DLPC7540EVM to control it. The DLP471TE DMD is not compatible with the DLPC4422 controller chip.
When you buy the DLPC7540EVM and the DLP471TEEVM separately, you get:
You don't get:
You will find on ti.com the following supporting collateral:
It would be best if you start by reading the Users Guide which provides information on what can be achieved with the EVM sets.
Lidong,
We don't provide compiling tools nor source code. We do provide a programmer's guide which shows what commands are used to control the DLPC7540 chipset. The programmer's guide has not yet been published as of to date. It will be available with the next firmware package install update that will be available on the DLPC7540EVM ti.com tool folder.