Other Parts Discussed in Thread: DLPC3436
Dear DLP community,
I have two furter questions regarding the DLP® LightCrafter Display 230NP EVM.
1.
I want to test the CAIC and created Phython commands as follows (inserted in the Python template script):
WriteLedOutputControlMethod(1)
WriteCaicImageProcessingControl(4)
While I don't get an error message, I don't see any effect. on the screen. Do I have the wrong argument numbers?
2.
The dlp 230NP EVM seems to have an optical actuator to get 1920*1080 resolution with 960*540 pixel. Is this actuator switched on by default? And can I switch this actuator on/off using a python script?
Thanks in advance,
Ulli