I am working to measure and monitor industrial liquids (wastewater, sanitation/CIP, product quality). I am curious if the DLPNIRNANOEVM is a good fit for our use case. Is there some kind of plug and play development kit available? What is the lead time to acquire a sensor for us to test it?
I am also wondering if you can provide any information on the lifespan of the sensor, the error range of the sensors, as well as any information on sensor reading drift. Furthermore, is there also any information on how long it takes for the sensor to capture a full spectra and if it can be used for liquids inflow. In particular, I am curious if this eval board works well with determining compounds in milk and if it is okay to use this board outside of the testing temperature range (0 to 50C) stated in the user guide for this product.
Thank you very much.