This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP230NP: EVM

Part Number: DLP230NP
Other Parts Discussed in Thread: DLPC3436, DLPDLCR230NPEVM

Dear Sir/Madam,
We have purchased the DLPDLCR230NPEVM, and we tested it using a power supply: 5V 3A. The spec on page 6 paragraph 4 states that when you power up the EVM it will display a logo. Also that the the D_HOST_IRQ will be OFF ( which indicates a successful boot of the DLPC3436), and that the D_DONE and D_INIT_B will be ON (to indicate a successful boot-up of the FPGA).

However the D_HOST_IRQ is constantly On, and the D_DONE goes On and Off and the image flashes momentarily. Does that mean that the FPGA and the DLP3436 have failed? please advice.