Hi:
I downloaded the VHDL files supplied in your dlpc103a zip file and ran the executable that installs all the files into the Documents/Texas Instruments/ folder. When I look in the folder the sub folder synchronizers with the associated synchronizer vhdl library file(s) is(are) not included. As a result, I have not been able to successfully compile the code into a working mcs or bin file using iMPACT in the Xilinx ISE developer software.
This file is specifically referred to in the user guide "DLP Discovery 4100 - Application FPGA Pattern Generator Design" on page 9, bottom paragraph:
There are two VHDL libraries, a "synchronizers" and a "ddc4100" library needed to compile the APPSFPGA code in addition to the default "work" library. ...and is located in the "<installation directory>/Software/synchronizers/" directory. ...which doesn't exist.
If you could point me to this library it would be GREATLY appreciated as I have spent a significant of time trying to make this work. If you could supply project or configuration files for the ISE, it would be even more appreciated but I will take the former if the latter isn't available.
Thanks,
Dave