Part Number: DLP2010EVM-LC
Can the micromirror array handle pulsed IR above 20 kW / cm^2?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLP2010EVM-LC
Can the micromirror array handle pulsed IR above 20 kW / cm^2?
Hi,
The power limit for the DMDs is based on the thermal capacity of the device, So if the 20kW/cm^2 is applied for a short enough period of time Its's reasonable that this may work
The high power may cause a temperature gradient in the DMD that may shorten its life span, and of course 20kW is far above the recommended power for this device, So TI cannot recommend you do this. you would need to do your own testing to verify this application
Regards,
Arthur
Hi,
I found this TI whitepaper which pertains to your application https://www.ti.com/lit/wp/dlpa027/dlpa027.pdf?ts=1629823476101&ref_url=https%253A%252F%252Fwww.google.com%252F
Regards,
Arthur