Dear Sir/Ma'am
This is regarding the DLPDLCR2000EVM: Projector Offset .Hope that a projector is made to have a offset value of 0%.Also I guess ,According to the construction and placement of particular projector , the offset are set. So is there any way to get a DLPDLCR2000EVM product projector with zero offset.