This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC900DEVM: Video pattern mode does not show the pattern consistent with the bit value

Part Number: DLPLCRC900DEVM

Hi Team, seeking for your assistance about DLPLCR9000EVM.

trying to use the DLP900EVM in video pattern mode at a frequency at 720Hz (30 fps * 2b bits) using HDMI port. 

We have constructed the video so that in each frame there are 24 1bit images.

For example for the frame with

R 00000001

G 00000000

B 00000000

I should see only one image fully white preceded by 7 black images and followed by other 16 black images.

This does not always happen, often my photodiode detects tho or three white images instead only one. The change time is correct and checked using the output of trigger 2 that change its value every time the 24RGB bit change).

We are convinced that the problem is due to the video streaming of our PC through HDMI because when we change the video player and or PC we notice different behaviours. Do you have any way of helping us to identify the parameters and suitable software for video streaming? Because at the moment the device is unusable. With what software do you guarantee operation in video pattern mode?

Thank you

-Mark