Other Parts Discussed in Thread: DLPC900

Hi everyone,
I am experimenting with SLM composed of DLP6500+DLPC900.Recently,I tried to perform grayscale calibration.I made a monochrome grayscale map of 0-255, and projected one sheet at a time.
1. I use a reflective DMD + external LED parallel light source, and the gray scale is discontinuous during projection, they change in steps. A typical point is that there must be a jump at 128bit, and linear changes cannot be achieved.
The camera exposure time is about 4ms, the projection exposure time is 100,000us, and the dark time is set to 80,000us. I see someone in the forum has achieved linearity by changing the camera parameters, but I did not get the ideal linear result by the adjustment. I think the reason is that I am not clear about the reason for the discontinuous grayscale change. So how should it be adjusted?
2. In addition, how many 8bit images can be projected at one time for the 6500. The effect of projecting 20 grayscale images at a time is different from that of a single projection 20 times. Each time the grayscale calibration is projected one by one is very time-consuming.
Hope everyone can help! ! Grateful! !