Hello,
There is a question of the DLP NIR Nano EVM develop would like to look for help.
The wavelength range is 900nm ~ 1700nm of current EVM model.
If we would like to change the wavelength range to maybe 1000 nm ~ 2000nm or 900nm ~2500nm.
For the firmware and software portion, what will need to modify based on current source code.
Assume the dlp speclib might be changed on both firmware / software (gui) side.
We are look for some advise so that we can speed up the study.
Thanks,
Paul