Hello!
Please make a firmware for dlpc2607 without image processing, please disable all image processing.
I am trying to create a projector for a black and white image. I only need a black or white pixel.
Vladimir.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
Please make a firmware for dlpc2607 without image processing, please disable all image processing.
I am trying to create a projector for a black and white image. I only need a black or white pixel.
Vladimir.
Hi Vladimir,
We apologize for the inconvenience, however, the DLPC2607 at this time does not support light control features.
If you are trying to display fully-white or fully-black image, then I would recommend using the i2c command to enable image curtain. No image processing is done on these curtains (these images are written directly to DMD). Information on this command can be found in the DLPC2607 software programmer's guide here: https://www.ti.com/lit/ug/dlpu013a/dlpu013a.pdf in section 2.4.1.17.1.
If you are trying to display specific test patterns, please see section 2.4.1.10 on i2c commands to enable and select your internal test pattern, however, there will still be internal image processing done on these images.
If you would like more control over what type of image processing is done on your image (structured pattern, etc.), we recommend using the light control chipset which can be found in this EVM: https://www.ti.com/tool/DLP2010EVM-LC.
Thank you,
Chris