I am looking for a DMD to buy for my basysprint machine. I cannot able to find part code to order.
I have a picture of the DMD for reference, kindly find out and update me.
Please find the attached Picture, which I am using the DMD.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Prema,
Sorry for the delay, this thread request did not come up in our correct queue.
Are you looking for another type A DMD with the 0.65 1080p resolution? If you provide more information, we can help.
Thank you,
Matt
This looks like the 0.7 XGA device. Our current device that is available is the DLP7000 DLP® 0.7 XGA 2x LVDS Type A DMD.
This DMD is controlled by the DLPC410 and uses the DLPR410B PROM.
Would you be able to tell us what controller and PROM version you are using? The current DMD I mentioned should be drop in compatible, but I will want to double check with the team here.
Thanks,
Matt
Hello Prema,
The DMD used is no longer manufactured.
Check the rev. of the PROM to see if it is rev. 4. If it is rev. 4 a DLP7000BFLP can be used as a replacement.
If not rev. 4 we can work to see if there is another option to replace the DMD.
Regards,
Matt
Hello Prema,
To add a little bit to Matt's post the PROM you are looking at should say DISCO3000-004 on a little white label on the controller board (I believe it is an 8 leg TSOP package PROM). It allowed the newer 2xLVDS 0.7 XGA DMD DLP7000(B)FLP to be operated at 1xLVDS speed (200 MHz).
Fizix