Other Parts Discussed in Thread: DLPC3436, DLP230NP
Hi,
I'm setting up DLPDLCR230NPEVM to connect it with the Raspberry PI
Specifically, I'm about to write the relevant firmware by executing the included scripts.
(flash_write_fpga.py, flash_write_controller.py)
However, in the contained dlpc3436_release_notes.html file, I can see the line saying
- Optimized Frame Rates: 60Hz (2D), and 120Hz (3D)
What I want to do is setting the resolution to the 960x640@240hz which is out of the "optimized frame rates"
Can I simply ignore this document and write the firmware?
Thank you.