This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2000EVM: By a SBC also a HDMI/DVI decoder

Genius 11110 points
Part Number: DLPDLCR2000EVM
Other Parts Discussed in Thread: TFP401

Hi team,



I have been trying to use DLPDLCR2000EVM in two ways, both failed to work:

1) by a Raspberry Pi 4b+ as described here: frederickvandenbosch.be/
also here: e2e.ti.com/.../dlpdlcr2000evm-connection-to-raspberry-pi-4-model-b
On the raspberry, after wiring and editing /boot/config.txt as described in the first link, I get the following

$ sudo i2cdetect -l
i2c-1   i2c             bcm2835 I2C adapter                     I2C adapter
i2c-7   i2c             ffffffff00000002.i2c                    I2C adapter
$ sudo i2cdetect -y 7
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- 1b -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- 57 -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --



Then running 

sudo i2cset -y 7 0x1b 0x0c 0x00 0x00 0x00 0x13 i

sudo i2cset -y 7 0x1b 0x0b 0x00 0x00 0x00 0x00 i

however the flash screen still is playing the splash screen

2) I used adafruit hdmi/dvi decoder TFP401 with a NHD-TFT40 new heaven board wired to EVM, where parallel RGB888 vid data pins were connected to the NHD-TFT40 pins, along with the VSYNC, HSYNC, DATAEN and CLCK pins. Then, through a Raspberry Pi, I sent the I2C commands above to the board.

In both methods, only the spalsh screen keeps playing. Could you please help me how to get some picture out of the DLP.

thank you.

Best regards,
William