This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP5530PGUQ1EVM: Support firmware

Part Number: DLP5530PGUQ1EVM
Other Parts Discussed in Thread: DLP5530Q1EVM

We want to understand DLP5530 firmware for our future design.

Could you please help to share the required firmware with us?

  • Hello - 

    Are you building a fresh set of electronics? Will the board design match the DLP5530Q1EVM design?

    There are certain parameters that may need to be adjusted in the firmware according to the electronics design.

    Thanks,

    Ross

  • Yes, we are building a fresh set of electronics. However, we are only planning the design scheme preliminarily at present, so we would like to know about the firmware information, so as to better design the products we want.There are no other requirements at the moment. Could you please help to share the required firmware with us?

  • Hello - 

    Hope to get the firmware you share with us as soon as possible!

    Thanks,

    yang

  • Hello Yang -

    The attached file is a standard firmware build that is compatible with the DLP5530-Q1 EVMs.

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/94/FlashImage_5F00_HUD_5F00_MultiRGB_5F00_MediumRed_5F00_DLPLogo.bin

    However, if there are additional configuration changes needed, then you will need to download a program that builds custom firmware, and for this task I will connect with you via email.

    Regards,

    Ross