This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC900: Dual Pixel Mode

Part Number: DLPC900


Hi Team,

 

From the datasheet for the DLPC900

“Each controller must operate in two pixels per clock”

 

This implies that to drive the 670S the DLPC900’s need to be in dual pixel mode.

Can you confirm that?

Thanks!

Connor

  • Hi Connor,

    Yes, the two pixels per clock mode is correct if the user wants to access all of the pixels on these DMDs ("dual pixel mode" is not a phrase we use in the documentation, but we get what you are referring to). The native resolution for these DMDs is higher than the display standard of WUXGA, so to maintain accurate data to the mirrors and to get good image quality, the system needs to be running as fast as possible.

    Hope this helps,

    Matt