Part Number: DLPR410
PCN regarding DLPR410BYVA describes "Mirror float and power float now result in a full park sequence". What do you mean "a full park sequence"?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
The DLPR410 [DLPC410] through version 5 had a power down park sequence (PWR_FLOAT) and a “mirror float” (recoverable flat state) command for the DLP7000 and DLP9500 DMDs.
DLPR410A v7 added support for the DLP650LNIR DMD. However, inadvertently the RST_ACTIVE assertion was eliminated for both PWR_FLOAT and “mirror float”. Some customers rely on this signal to tell them when a reset or park pulses are active.
The DLPR410B firmware moves the functionality back to the DLPR410 v5 operation, please adds a few timing adjustments that are required to meet the proper floating of the mirrors either before shutdown or recoverable “mirror float” operation.
Please let us know if this explains the changes.
Thank you,
Matt