Part Number: DLPDLCR3310EVM
Hi Team,
Seeking some information
With short focus distance about 10 - 13 centimeters, are there any compatible optics? It is possible o replace it?
Thank you.
-Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLPDLCR3310EVM
Hi Team,
Seeking some information
With short focus distance about 10 - 13 centimeters, are there any compatible optics? It is possible o replace it?
Thank you.
-Mark
Hello Mark,
Welcome to DLP forum and thank you for your interest in DLP technology.
With short focus distance about 10 - 13 centimeters
Do you mean the minimum focus distance for an optical engine? Or an Ultrashort engine where you create large size form this distance?
Based on your application need , you need to define the following parameters for your optical engine:
1. Brightness
2. Throw ratio
3. Offset
You can refer to following application notes on " TI DLP® Pico System Design: Optical Module Specifications "for definition of these terms:
Once you have specification ready, please use 'DLP-OMM_SEARCH" tool to identify the optical engine available for our third-party network.
https://www.ti.com/tool/DLP-OMM-SEARCH#description
Please contact the manufacturer directly for the optical engine.
Please note that the interface (*connector & signal connections) are defined the engine manufacturer and may not be compatible with the TI EVM. In that situation, you have either design your own board or ask them or an hardware board.
Hope this answers your question. Please let us know if you have any follow-up questions.
regards,
Vivek