Other Parts Discussed in Thread: DLP7000, DLPC900, DLP9000, DLP9000X
Hello,
Is it possible to get approximate current consumption of the DLPLCR65EVM board. We are using this board
From the datasheet the power requirements are in Section 5.1 Nominal voltage: 12-V DC; Maximum Current: 7 A; and the recommended power supply is Digi-Key part number 102-3811-ND, which is 5A
The actual current measurement I have made was 0.48A
We are only using display port for imaging and USB for a control
Best regards,
Timur