Other Parts Discussed in Thread: DLP2010LC, , DLPC3478
Hi All,
We have been successfully using the 3470/2005/2010 combination in a structured light application for several years now. We operate the device with the input trigger enabled to synchronize it with a image sensor. This is working well for us.
We are now investigating a new mode of operation that requires us to reactivate splash display mode after stopping internal streaming and are having problems getting the 3470 back into splash screen mode after it has been in internally streaming images.
We recorded these commands using the evaluation board to switch from int pattern streaming back to splash screen 0:
W 36 05 04
W 36 9E 00 FF
W 36 9E 01 00
W 36 1A 01
W 36 2E 56 03 E0 01
W 36 10 00 00 00 00 56 03 E0 01
W 36 12 00 00 00 00 56 03 E0 01
W 36 90 00 <tried adding this to disable the internal triggering mode
W 36 0D 00
W 36 05 02
W 36 35
W 36 52 07
W 36 1A 00
But when I write code to generate these same commands, the projector remains in streaming mode. I am delaying 10 ms between each written command.
I also tried disabling the internal trigger with the extra command, but that didn't help.
Any suggestion are most appreciated.
Thanks,
Scott