This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA2005: Setting LED Current to 2Amp

Part Number: DLPA2005
Other Parts Discussed in Thread: DLPC3470, DLP3010EVM-LC, DLP2010LC

Dear TI, 

Resently, I am tsesting my DLPA2005 + DLPC3470(firmware version: dlp2010evm-lc_7.3.1) +  DLP2010A FQJ+ LE B Q8WP application(Based on DLP2010EVM-LC) 

Tyring to set the LED current to 2A by sending these commands.

Write RGB LED Current PWM (54h)

Write RGB LED Max Current PWM (5Ch)

The Maximun current I can get is about 1000mA(0x0194), higher LED currnent settings will rising the anode voltage of LED to about 6V, with 1000mA LED current.

It seems that DLPA2005 is in  VLED Overvoltage (VLED_OVP) Fault conditon. 

I noticed that the DLP3010EVM-LC is capable for 2.4A LED current by changing the Inductor of LED Driver. Is it possiable to get similar current with DLPC3470+DLPA2005?

Or the firmware version is not correct? Because I tried on several different PCB and LEDs, the Maximun current is 1000mA aswell.

Could you give me some suggestions?

Regards!