Hi,
I would like to know the output current accuracy of ILLUMINATION DRIVER A/B of DLPA3005.
The following pins also function as output pins, so please tell me the output current accuracy for these terminals only (not including external circuitry)?
ILLUM_HSIDE_DRIVE(26 pin)
ILLUM_LSIDE_DRIVE(27 pin)
ILLUM_A_SW(31 pin)
ILLUM_B_SW(36 pin)
ILLUM_A_COMP1(38 pin)
ILLUM_A_COMP2(39 pin)
ILLUM_B_COMP1(40 pin)
ILLUM_B_COMP2(41 pin)
Best Regards,
UNA