Hi,
We have DLP requriement for HUD which is auto grade
But the requirement is Full HD resolution , TI has no full hd auto grade IC
so i was looking at pico chisets in which DLP4710 was having temperature range of -20 to 90 which is good and better
but only thing i am not clear is are these pico chipsets suitable for HUD kind of applications
or can use a full HD supported standard chipset and use a heater to achieve lower temperature operation which is -40 degree
kindly suugest best possible solution