This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP Guide: Which TI dev't kit would be suitable?

Genius 17865 points
Other Parts Discussed in Thread: DLP3010EVM-LC, DLP4710EVM-LC

Hi Experts,

We have this query from Cx about DLP:

I am currently working on a project where we want to control a DMD using a PC through high-speed visual feedback (500~1000Hz). The DMD is supposed to change the path of a laser beam in the visible spectrum and a power of 80 mW.
I checked the DLP development kits, but since I am completely new to DMDs I couldn't decide which one would be suitable for our application. My question is: can we control the DMD (only mirror, no need to control LEDs) with 1KHz frequency using C++ code running on a Windows PC, for example through USB, without using Rasberry Pi. 

If it is possible, what kits do you suggest?

Thank you

Regards,
Archie A.