Part Number: DLP3030-Q1
Dears,
I have some questions about Photodiode selection
1. Are there specs on Photodiode? Are there selected criteria and conditions?
2. Is there any restriction on the placement of Photodiode in the optical machine (where can it be placed)?
3. Is it possible to not use Photodiode on the DLP3030-Q1 architecture?
4. If needed. The reason why DLP3030 needs to add Photodiode?
5. Is there a meter for photodiode signal strength corresponding to brightness (R/G/B LED current), color temperature?
Many thanks & Best Wishes
Weite
E:weite.chi@ofilm.com